5/29/2014 10:28 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello Amit Welde Unfortunately life with CFC ( PCS7 ) is not so easy as it is with a standard S7-400H. In a S7-400H system ( Without CFC ) you can make most downloads without both CPUs going to STOP Mode ( By following proper download sequence ) However Downloading CFC to a H system is quite another ballgame.Most Major changes ( Changes in Block interface, Interconnection etc ) would call for a full download and both CPUs will go to STOP. This at times defeats the very porpose of a H system. However if you are careful, you can reduce this condition ( If not avoid completely ) The Following FAQs include some information and Tips for avoiding such situations. ES - SIMATIC Manager -- Working with projects -- Compiling / Loading PLCs Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
5/29/2014 10:33 AM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (22) |
Have you check with the diagnostic buffer and can you post here. We can check what is the problem ?? Program ?? |
6/2/2014 5:59 AM | |
Joined: 12/2/2013 Last visit: 1/12/2023 Posts: 34 Rating: (1) |
sorry for late reply, i want to download the "changes only". and i m not using PCS7. |
6/2/2014 9:23 AM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (22) |
Changes Only was enabled during download or you have only option of entire download ??? In the manual read Chapter 3.12 to know more about Changes Only and Entire Program.
AttachmentCFC_For_S7_e.pdf (105 Downloads) |
6/2/2014 9:53 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
HelloAmit Welde,
Wouldn't make much difference because the download restriction comes from the nature of CFC not from being PCS7. As described earlier that some changes may require a STOP of both CPUs. So, we can't speculate the reason as long as we don't know what changes you have made and download procedures you have followed.
Best regards, H-H
|
This contribution was helpful to3 thankful Users |
Follow us on