5/27/2014 1:45 PM |
|
Joined: 5/12/2014 Last visit: 9/9/2020 Posts: 149 Rating: (16) |
Dear, Is there any contruction wise difference of DC motor & DC generator?? |
5/27/2014 4:27 PM |
|
Joined: 10/10/2010 Last visit: 9/14/2024 Posts: 307 Rating: (15) |
the construction of the commutator device is diffirent and the field winding also diffirent |
5/27/2014 4:38 PM |
|
Joined: 4/20/2007 Last visit: 9/19/2024 Posts: 727 Rating: (43) |
Seeherefor some more info. |
5/27/2014 6:53 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello Chetan2490 Practically every DC Motor can also be used as a Generator. Here is a very simplified description : Basically, if you excite the DC Motor Field and apply Voltage to its Armature, it will start rotating as a motor ( and also rotate the load copupled to it ), The Speed is proportional to the Armature Voltage upto Base Speed and thereafter if the Motor is designed for field weakening then you can increase the speed further by reducing the field current ( This is however not a linear but a Parabolic type of charactristic. ). On the other hand, if you if you excite the Fieldand couple the same motor to a prime mover ( an engine, turbine, a mechanical flywheelor another motor ), then it will act as a generator. Armature voltage will be proportional to the speed at which it is being rotated. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
5/27/2014 7:03 PM | |
Posts: 28 Rating: (4) |
Dear, Is there any contruction wise difference of DC motor & DC generator?? hi there are NO constructional difference of DC motor & DC generator. regards aakash |
5/28/2014 7:40 AM |
|
Joined: 5/12/2014 Last visit: 9/9/2020 Posts: 149 Rating: (16) |
Thank you very muchNavnag. Your Answer is really Helpfull
|
6/2/2014 9:34 PM |
|
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating: (9) |
Same person & same questions all around the forum |
Follow us on