6/12/2014 4:10 PM | |
Posts: 2930 Rating: (432)
|
Dear LOGO! friends, attached is an example how to show times in the display as bargraph.Used products: LOGO! 12/24RCE LOGO! Soft Comfort V7.1.5 Issue: The bargraph doesn’t support running time of an Off-Delay (for example). This FB cannot be selected in the selection list of the bargraph. Sollution: The trick is to transfer the value to analog amplifier for example. The value of a anlogue amplifier then can be used for the bargraph. I solve this by transferring the value via the VM-mapping table to the V-Memory and then use analogue network input to read it back and forward it to a analog amplifier. The value of the analog amplifier can then be used for the bargraph.Have funn testing my example. Regards HElmut AttachmentOff_delay_Bar.zip (264 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on