4/23/2012 2:56 PM | |
Posts: 3037 Rating: (192)
|
Hello, You can see all cable and adapterwhich you can use to the download to a panelin the following FAQ. What transfer options are available in the various operator panels? Other cable or adapter can work or not. Tweety |
4/23/2012 5:01 PM | |
Posts: 6 Rating: (0) |
Thanks for the answer, but i find it strange that the new version does not work (only for update OS) with my adapter hilscher.
|
4/24/2012 11:20 AM | |
Posts: 3037 Rating: (192)
|
This adapterwas not tested. You have luck that the adapter works in the previous version of WinCC flexible. You do not need the version SP3 of WinCC flexible absolutely, you can useWinCC flexible 2008 SP2. Tweety |
4/24/2012 11:36 AM | |
Posts: 133 Rating: (9) |
Hi Brad I'm sure you have already checked the cable that you are using for the different cables. Check out the attached document if you are definately using the correct cable. AttachmentTransfer Cable Options.pdf (167 Downloads) |
6/17/2014 12:25 PM | |
Joined: 3/2/2007 Last visit: 3/20/2024 Posts: 917 Rating: (5) |
so , which cable should be used for OS update on TP177B ? |
... thank you ... |
|
6/17/2014 2:19 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (704) |
Hello Ziemens, Please have a look: Which connector cables are available for connecting to SIMATIC Panels? |
Follow us on