6/19/2014 3:55 AM | |
Posts: 20 Rating: (0) |
Hi I have a ET200M module (153-2AA02-0XB0). i can't find GSD flle. Plese help me.
|
6/19/2014 5:46 AM | |
Posts: 20 Rating: (0) |
Hidchartier I am using TIA porttal, i can't find it in catalog.Yesterday I installed the GSD file but I only find 153-2BA02-0XB0 not 2AA02
|
6/19/2014 5:54 AM | |||
Joined: 9/27/2006 Last visit: 5/11/2024 Posts: 12257 Rating: (2666)
|
Hello Jack; The 6ES7 153-2AA02-0XB0 was discontinued in 2011, and replaced by the 6ES7 153-0BA02-0XB0. See the Product Support page for this product in the link below. In any cse the gsd file is in the link provided earlier, marked as Order no.: 6ES7 153-2*A0*-0XB0 Hope this helps, Daniel Chartier
|
||
6/19/2014 6:03 AM | |
Posts: 20 Rating: (0) |
of couse,So how do I use the old versionmodulein TIA ? |
6/19/2014 4:29 PM | |
Joined: 9/27/2006 Last visit: 5/11/2024 Posts: 12257 Rating: (2666)
|
Hello Jack; The module for which you have the gsd file in TIA Portal is a replacement module for the IM 153-2 you actually have. This means that they are functionnally the same, with variations in the electronics boards. So you could try first to set the older module with the new gsd, test it with your module and see if the DP-master accepts it, or if it gives an error. If the master does not accept it, try importing the older version of the gsd file in your TIA Portal: How to install GSD file on tia v11 Hope this helps, Daniel Chartier |
Follow us on