6/17/2014 7:20 AM | |
Posts: 1299 Rating: (135) |
Hello, did you install the latest graphics driver? K!ke |
6/17/2014 10:45 PM | |
Joined: 5/24/2012 Last visit: 2/19/2024 Posts: 70 Rating: (0) |
Yes I have installed the latest drivers from intel |
7/15/2014 6:04 PM | |
Joined: 10/18/2012 Last visit: 12/15/2023 Posts: 225 Rating: (23) |
Ah, ok. I didn't get that fact of two identical IPCs connected to two monitors. Unfortunately I have no idea what could cause this problem. Could you connect the 55inch monitor via a different type of cable, i.e. DisplayPort or HDMI? Maybe sending the signal from the IPC through an adapter into another type of cable and to the monitor makes a difference. If nothing helps at all, try to contact Siemens Support and describe them your hardware setup in detail. - edited support-request link |
Last edited by: xnor at: 7/15/2014 7:38 PM |
|
This contribution was helpful to1 thankful Users |
7/15/2014 6:36 PM | |
Joined: 5/24/2012 Last visit: 2/19/2024 Posts: 70 Rating: (0) |
I'll try swapping with a different kind of cabe Thank you for the help |
Follow us on