7/15/2014 1:43 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Hello Lukas; This sounds like a problem we Profibus users do not meet very often. It is more of a developper issue. If you do not get enough help from the forum membershere, then I would like to suggest the Profibus.com forum, which is specialized for developpers of Profibus and Profinet communication partners: http://www.profibus.com/community/forum/discussion-board/ There is also a bit of information available on RedCom issues: - From the Siemens forum: about Flying redundance - Siemens Industry Online Support - Information from the Profibus.com technology pages Slave Redundancy - Profibus International Competence Center Hope this helps, Daniel Chartier |
Follow us on