Industry Online Support
Technical Forum
6/29/2014 10:33 AM | |
Posts: 5225 Rating: (1192) |
Hi there. Welcome. The software you speak of (I think) is Sinamics StartDrive. This software is bundled with TIA Professional V13. This software will not be of help to you when you wish to use a MicroMaster. As to your second question.. There is a strict method to follow to get the hardware caterlog updated. I do not have experience with TIA V12. I recommend you ask that question within the groupSTEP 7 (TIA Portal) Greetings. w |
6/29/2014 9:46 PM | |
Posts: 5 Rating: (0) |
Dear William Thank you for your replay Mzsa |
This contribution was helpful to1 thankful Users |
6/30/2014 7:17 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, if you can help: LIBRARY FOR S71200MPLC ON USS COMMUNICATION WITH MM420 |
Last edited by: Ste39 at: 6/30/2014 7:19 AM |
|
7/18/2014 6:19 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328) |
But the better solution is to update to STEP7 V13 and Startdrive V13 (same downloadpage, but article number 6SL3072-4DA02-0XG0) MICROMASTER IS NOT SUPPORTED IN STARTDRIVE! You must use Starter to parametrate the MM. To be able to add it as slave to the PROFIBUS, it may be necessary to import it via a GSD file. |
Last edited by: miami at: 7/18/2014 6:25 PMLast edited by: miami at: 7/18/2014 6:24 PM |
|
Follow us on