Industry Online Support
Technical Forum
8/3/2014 5:32 PM | |
Posts: 4 Rating: (0) |
Dear Experts, Im facing problem on S7-400 hardware configuration compile error. would like to clarify that the machine is running since 2005 and there was no issue. Recently we were trying to add few diagnostic repeaters on current hardware. When i add the repeater on my profibus network it gives compile error. So i have removed it and try compiling again. Still i face the same problem (pict 1). for testing purpose i upload the program from CPU and compile the hadware without any changes but it give the same error " compile inconsistance". Please advice. i have tried with 3 Step 7 laptops all giving same error. even with siemens PG. Step 7 V5.5 sp1. Dhivaharan
AttachmentPICT.zip (79 Downloads) |
Follow us on