Industry Online Support
Technical Forum
8/13/2014 8:02 AM | |
Joined: 8/25/2006 Last visit: 5/8/2024 Posts: 2203 Rating: (277) |
Hello. By default there are 2 DI's that (X177:12, 13) have a function ON/OFF1 and Enable/Disable pulses. There 2 free DI's (X177:11, 14) and you can also use bidirectional DI/DO (X177:15-18). There are also 6 AI's. Look at theList manual, function diagrams. You can program any required logic using DI's and/or AI's. UsingStarteris not necessary, but this is the easiest way for programming drive.
|
Follow us on