8/20/2014 12:37 PM | |
Joined: 10/26/2011 Last visit: 4/22/2024 Posts: 760 Rating: (190)
|
Hello In the process industry, a common use of the electronic weighing system is the dosing of one or more substances in a reactor. Therfor an application example and a project exampleare available. The application example as well the project example are based on the PCS 7 APL library and the SIWAREXFTA PCS 7 add-on library. http://support.automation.siemens.com/WW/view/en/98754973 Customer benefits When using the SIWAREX FTA - Advanced Process Library you also get the following benefits:
|
Last edited by: CS Moderator at: 8/23/2014 9:54 AMAttachment reattached Last edited by: Thunderstorm at: 8/20/2014 12:42 PMSIMATIC PCS 7 - Overview |
|
Follow us on