Industry Online Support
Technical Forum
8/26/2014 11:41 AM | |
Posts: 664 Rating: (17) |
Hai All, I have to add a guage into the screen[KTP600 Basic PN],in tool i dint gent any guage option. Please give an idea.. Thanks&reagrds, Raj |
8/26/2014 12:20 PM | |
Posts: 664 Rating: (17) |
Hai eisenpferdreiter and Kahl, Thanks for the effort. I am working with WinCC flexible 2008,and HMI is KTP600 Basic colour PN. I didnt see any guage option in tool bar. If i changed the HMI type, it showing Guage option. Is there is any other otion to import the Guage option to screen with properties. I have to show the current varying in a motor to the guage. Is there any option.??? Thanks&Reagrds, Raj |
Last edited by: Karnan at: 8/26/2014 12:21 PM |
|
8/26/2014 12:28 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147)
|
Hello Karnan, Please have a look at the following link: What are the functional differences between the different SIMATIC panels? When you use a BASIC Panel, it is not possible to use a Gauge. Best regards, Wizard |
Follow us on