Industry Online Support
Technical Forum
9/8/2014 5:59 AM | |
Joined: 9/5/2014 Last visit: 3/1/2024 Posts: 6 Rating: (0) |
Dear Sir Pls. Help me I wants to change the old model OP17 to New OP177B Because the old one is obsolescence The old OP17 is connected to S7300 station CPU 315 via MPI and the station also had FM357 (Position Module) to control servo drive brand Movidrive,the old op17 have the project which write by Protool software , and the New OP177B might use the winCC flexible 2008 to write, first , I open winCC flexible and open the old project file and found ,then have windows to migrate the old project file to WinCC flex file (pls see picture in attaced file) and after I click next I found the error migration E3412 (pls see picture in attaced file) The detail is in attached file pls. advise me , how to solved this problem AttachmentSimens_Support_FM357.pdf (210 Downloads) |
9/8/2014 6:44 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello SomNaMon, Have you already seen this perhaps might help you: Conversing problem to WinccFlex 2008 What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)? |
Last edited by: Ste39 at: 9/8/2014 6:58 AM |
|
Follow us on