7/3/2009 9:41 AM | |
Posts: 14 Rating: (0) |
Dear all, Can i use common dc bus system and connect to S120 Motor Modules? TQ |
7/3/2009 11:01 AM | |
Posts: 160 Rating: (16) |
The sinamics S120 drive system is a multi-motor system so yes you can connect S120 Motor Modules to a common DC bus. However you need to take into account the number of drive objects that you are using. I would try to setup your configuration with Sizer to see what you can achieve with your modules You can dowload sizer from the following link. http://support.automation.siemens.com/WW/view/en/35401312 |
7/4/2009 8:55 AM | |
Joined: 9/18/2006 Last visit: 5/3/2024 Posts: 589 Rating: (64) |
Hi. Best regards. AttachmentCurrent carrying capacity of the DC link busbar.pdf (275 Downloads) |
7/6/2009 8:10 AM | |
Posts: 14 Rating: (0) |
Dear RAM, what do you mean SLM ? i want to use common DC busbar that from old Simovert P, it is possible? |
9/12/2014 2:37 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by cenkayais split to a separate thread with the subject how can i select the suitable smart line rectifier module? Best regards Min_Moderator |
Follow us on