6/2/2014 8:30 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Hellokire, There are 4 kinds of active busmodules. 1-6ES7195-7HA00-0XA0to integrate one IM and PS 2-6ES7195-7HD10-0XA0to integrate two IMs as in your case 3-6ES7195-7HB00-0XA0to integrate 2 modules each has 4cm of width 4-6ES7195-7HC00-0XA0to integrate one fail safe module with 8cm width. You can know how many bus modules your system requires when you make your hardware configuration (Properties of ET200M- Operating parameters)
You require one6ES7195-7HB00-0XA0for each 2 modules which means 3 in case of 5 or 6. Don't forget the one6ES7195-7HD10-0XA0for IM/IM. Best regards, H-H |
Last edited by: H-H at: 6/2/2014 8:39 AMEDIT: Corrected part numbers. Thanks Ayman Elotaify Last edited by: H-H at: 6/2/2014 8:33 AM |
|
6/2/2014 8:35 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835)
|
Hello,
For your case, you will need to install One bus unit "6ES7195-7HD10-0XA0" for the two IM 153-2, and One "6ES7195-7HB00-0XA0" for each two IO modules. For 5 or 6 IO modules, you have to install three bus units "6ES7195-7HB00-0XA0". To save money, when ordering the 2 IM153-2 "6ES7153-2BA02-0XB0" + 1Bus unit "6ES7195-7HD10-0XA0", you can order RED-Bundle which consists of 2 IM153-2BA02 + 1 BU IM/IM with one part number "6ES7153-2AR03-0XA0". Hope this helps.
|
Ayman Elotaify |
|
9/12/2014 4:17 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by SockeTis split to a separate thread with the subject How can I read the diagnostic of one profibus header?. Best regards Min_Moderator |
Follow us on