Industry Online Support
Technical Forum
9/11/2014 10:15 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Is this new or old running machine? Have you checked the DIP switch setting on infeed module? If 3 phase 400 Volt is available at main input terminals, 3 no GREEN LED should lit on, (see attached file) If it doesnot lit even if supply is available at power terminals, it signifies, problem with infeed module. HTH. AttachmentInfeed module LED significance.pdf (464 Downloads) |
Follow us on