Industry Online Support
Technical Forum
9/22/2014 7:58 AM | |
Posts: 9 Rating: (1) |
Hi How do I assign the identical blockicon to differnt pictures on the same tree that not to eliminate after compile on one of picture? Regards |
9/22/2014 8:27 AM | |
Posts: 767 Rating: (69) |
Hi bara1351, There is no standard option with flexible generation of multiple copies of block icons. There are two options possible for as far I know to solve your problem: 1. You can derive picture objects from lower hierarchy levels. But then you will derive all the block icons from selected lower levels. This is a setting in the Plant Hierarchie settings. 2. Generate 1 block icon and copy it by hand to the other picture. Modify the parameter "Type" of the block icon in Graphic Designerto something else (like removing the '@'). The only issue with this solution is that this copy must be removed by hand again when t is obsolute. Regards, Cedric |
This contribution was helpful to4 thankful Users |
9/22/2014 9:02 AM | |
Posts: 9 Rating: (1) |
Hi molthoff I appreciate it Second solution is great. Thanks a lot
|
This contribution was helpful to1 thankful Users |
Follow us on