9/3/2007 9:12 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hello, Have you seen this faq: http://support.automation.siemens.com/WW/view/en/15389520 Like Aret mentioned, the size depends on your programm. When you want to use the complete work memory, you should choose a Flash Eprom size which is bigger. So when you have a work memory of 48 Kbyte, you can use a Flash Eprom of 64 Kbyte. When you want to do Firmware updates, you need a Larger Flash Eprom. Best regards, Wizard |
10/25/2007 11:51 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hi, When you want to load complete project to MMC including comments and symbols, just have a look at following faq: http://support.automation.siemens.com/WW/view/en/15399111 Remember: you'll have to archive the project and put zip-file on MMC. In that case the MMC must be large enough for project and zip-file. Best regards, Wizard |
Follow us on