9/28/2014 3:14 AM | |
Joined: 10/7/2005 Last visit: 9/21/2024 Posts: 3021 Rating: (1054) |
Hello Arunraje firstly, fully agree with what Daniel said. As for your addendumquestion:
256 Profinet IO devices isthe limit for the current generation of H-CPU's (see also thetechnical spec of your chosen H-CPU). While this may be enough for you, note that the SIMOCODE PRO V PN does NOT (yet) support System redundancy! (see alsoits tech spec HEREfor more) This means it would be a unilateral PN IO device that only belogs to one of the H-CPU's. I'm hopefull Siemens is feaverishly working on adding System redundancy to a number of their PN IO devices (one must never loose hope), but as it stands, only the IM153-4 does support this so you are arguably better off using good old Profibus and Y-Links. I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on