10/7/2014 11:02 AM | |
Posts: 38 Rating: (0) |
Hello Expert, here i have attached F42 Trace file, if something possible to findout from this. Regards, Meet
Attachmentpinchroll f42.zip (336 Downloads) |
10/7/2014 11:26 AM | |
Joined: 8/25/2006 Last visit: 4/26/2024 Posts: 2203 Rating: (277) |
Hello. It looks like .trc-file is different from .wmf-file. Please upload the right .trc.
|
10/9/2014 9:16 AM | |
Posts: 38 Rating: (0) |
Dear Expert, pls find attachment
Attachmentf42.zip (232 Downloads) |
10/9/2014 1:17 PM | |
Joined: 8/25/2006 Last visit: 4/26/2024 Posts: 2203 Rating: (277) |
Hello. Is your drive 1Q or 4Q? Specify order number.
|
10/9/2014 2:02 PM | ||
Posts: 38 Rating: (0) |
Hello KSN,
Attachmentpinchroll parameter.zip (187 Downloads) |
|
10/9/2014 3:56 PM | |
Posts: 38 Rating: (0) |
Hello KSN, pls fine right file attached here (that one for other pnr by mistake attached wrong file last time), motor 15HP, Armature Voltage 500volt, Armature current 26Amp, 850/1000rpm,Field Current 2.26/ . Regards, Meet Attachmentpinchroll f42.zip (224 Downloads) |
10/9/2014 5:02 PM | |
Joined: 8/25/2006 Last visit: 4/26/2024 Posts: 2203 Rating: (277) |
Hello. First problem that I could find from your parameter list is negative current limit P172=0%, so your drive acts like 1Q, it could not follow the speed setpoint. As I see from trace, it looks like material still moving after the speed setpoint is zero, and material rotates the pinch roll, it has P172=0% and could not stop, that's why I think the F042 occurs.
|
This contribution was helpful to1 thankful Users |
Follow us on