10/26/2012 2:25 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
The S7-CPU and Sinamics can or use a communication with Profibus or Profinet. Both systems are bus connection with a detailed description how a Master and Slaves have to communicate using a special physical envinronment. A telegramm between Master and Slave is seperated in several PZD - in several words - where the user has to put in the information for the slave (drive) and where he gets the status informations. In a List manual for Sinamics S120 you can find a description about the available telegram and their PZD built order. If you select the right telegram in S7-CPU and in the drive then it is clear which information you have to send and which information you can receive. The standard functions SFC14/15 can be used for a telegram communication .
Have a look on the list manual.
|
With best regards, |
|
This contribution was helpful to2 thankful Users |
5/8/2013 4:26 PM | |
Posts: 2 Rating: (1) |
is stw1 and zstw1 is address? if not then can anyboddy tell me what should be the address..... |
5/8/2013 7:01 PM | |
Joined: 3/25/2008 Last visit: 8/12/2024 Posts: 57 Rating: (0) |
Hello, how ist posible to writte parameters in the comunicatios, chanching a parameter value?? enku |
5/10/2013 10:56 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, If you mean a cyclic communication then you have for many telegrams a (user)defined datablock. This datablock and its informations -which the user is changing in his standard programm - is send via for example SFC14/15 to the drive. If you want to change a parameter which is NOT part of your cyclic transfer - because this parameter is a configuration parameter - then you are using an acyclic communication with for example SFC 52/53. Additional informations can be found here (chapter 10"communication"): http://support.automation.siemens.com/WW/view/en/68042590 |
With best regards, |
|
8/30/2014 1:25 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
... that`s correct. |
This contribution was helpful to1 thankful Users |
10/16/2014 3:17 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on