Industry Online Support
Technical Forum
10/21/2014 2:05 PM | |
Joined: 9/16/2014 Last visit: 11/16/2023 Posts: 12 Rating: (0) |
InWhich connector cables are available for connecting to SIMATIC Panels?, it is indicated that the cableUSB PC adapter (I suppose that mine is) isreleasedfor the device KTP600 Basic Color DPfor project transfer and OS updating, but it's not indicated the way for doing that. Any idea how do I have to do that? What's the configuration?
|
10/21/2014 2:34 PM | |
Posts: 1058 Rating: (93) |
Hello gusbarciela, have you put your panel into transfer mode before you started downloads? If not, you should try that. regards |
10/21/2014 4:10 PM | |
Joined: 9/16/2014 Last visit: 11/16/2023 Posts: 12 Rating: (0) |
Yes, I have put the panel into transfer mode before downloads. Thanks anyway.
|
10/21/2014 4:35 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello gusbarciela, How are the LEDs on the PC adapter? 16983464 Have you already seen this: How can you transfer a WinCC flexible project via MPI/PROFIBUS |
Last edited by: Ste39 at: 10/21/2014 6:17 PMLast edited by: Ste39 at: 10/21/2014 5:48 PM |
|
10/21/2014 6:49 PM | |
Joined: 9/16/2014 Last visit: 11/16/2023 Posts: 12 Rating: (0) |
Yes, the leds are on. But I have read"Howcanyoutransfera WinCC flexibleproject via MPI/PROFIBUS",and there is indicated the next:
I suppose this is the reason because I can't transfer the project. Thank everybody.
|
Follow us on