Industry Online Support
Technical Forum
11/4/2014 9:57 AM | |
Posts: 122 Rating: (1) |
Hello Experts, I have to send a signal or say Memory bit to PC. The PC has a application which would read the data from the PLC and put it in a database which is located in a server for assessment. I am using S7 1200 TIA portal . Last time when I tried to connect it said an error that there is no available ports or no ports were free in the PLC to get connected. I read throug the forum and from googling understood that there has to be a setting made. I have done the settings for TSEND_C instruction. But could not check whether it is correct. If any experts who could correct if any thing wrong would be nice. Unfortunately I could not test as the PC application softwre which would read the data from the PLC is located elsewhere. And cannot access every time to test it. But today it is possible to test after an hour or so. I want to eliminate errors before that so that I can save time. Looking forward to your support and opinion. I have attached a zip file where you could find the snop shots with regard to my question. With regards Johannes
AttachmentZipFile.zip (378 Downloads) |
11/5/2014 10:47 AM | |
Posts: 122 Rating: (1) |
Hello Expert, Thank you for your suggestion and observence. I shall check and if any further questions I shall post. With regards Johannes
|
Follow us on