11/6/2007 6:16 PM | |
Posts: 20 Rating: (0) |
Thank you vey much! I will show you the userguide of the profibus-dp card as files attachment, please see at second page! it request Profibus-DP V04 ! please help me best regard! AttachmentInfo_Communication_modules_HWRev4_en_2.pdf (524 Downloads) |
11/6/2007 11:17 PM | |
Posts: 5822 Rating: (412)
|
Hello, ohh... I guess now I got the point! I fear the important point in her is the headline in your list. There it is mentioned that you need from the HW Version 3 on the Firmware that is called PROFIBUS DP V04, but this is a Firmware by the SIPROTEC 4 Communication module you use... This is a device of the PTD Department. I hope you will get some more information’s there. Best regards J_Bell |
11/7/2007 2:36 PM | |
Posts: 20 Rating: (0) |
Thank you for your help! But, May you explain for more detail, i still don't know clearly what you want to say, i am using theprotect device has HW Version 4 such as 7SJ62, 7UM61,... i also read the manual of PTD as file attachment to by Profibus-DP module has order No. C53207-A351-D611-1 and bought it. I also configrued on the Protection device by DIGSI 4 software for address and mapping file. Please help metoconsiderthisproblem. AttachmentOrdering information for_communication modules_2.pdf (483 Downloads) |
11/7/2007 3:09 PM | |
Posts: 5822 Rating: (412) |
Dear hanhdn, this is a Forum for A&D Products... not for PTD Products, if you have such detailed questions to PTD Products you may have to ask PDT for it. J_Bell |
Follow us on