11/25/2014 2:46 PM | |
Posts: 8 Rating: (0) |
Thank you for your assistance thus far. To answer your main question, the template had a folder that contained .arc files as well as some documentation. I've attached a zip of these files in their folders and I hope that clears things up. I'm unfamiliar with the file structure of the compact flash and not sure if these files can be placed on the compact flash of the drive, or if a .usz file created using these files with CMC is all that goes on the card. It's unfortunate that my counterparts who gave me the template are unable to help me. Thus, I really appreciate your help.
AttachmentNC.zip (323 Downloads) |
11/26/2014 1:31 PM | |
Posts: 8 Rating: (0) |
CNC600, I really appreciate your help. I did not attach the PLC file as I thought there would be no issue there (though I'm struggling to load it as well). I created the .uaz file as you explained and have attached it here in case you have any interest in looking at it. When you mention reading in the OP010_NCDP_20141018_ASL.arc file, is this done from the HMI or from another application? Again, I greatly appreciate your help. AttachmentNC_NOEXE.zip (234 Downloads) |
Follow us on