11/27/2014 4:56 PM | |
Posts: 2 Rating: (0) |
Hello I am new user of PLC, my problem is i can't able to make continous pulse on my step 7 software with adjustable duty cycle. Please inform me what is the best approach?
------------------- New subject after splitting from pulse generator that input is starting, and count these pulse. |
Last edited by: Min_Moderator at: 11/28/2014 9:10 AMSplitted |
|
11/27/2014 5:22 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
Hello Rayhan, About the possibilities , I can think of :
AN M 10.0 I hope this helps, Hamid Hosseini |
Last edited by: hdhosseini at: 11/27/2014 5:23 PM |
|
11/28/2014 4:01 PM | |
Posts: 1058 Rating: (93) |
Hello Rayhan, what kind of pulse are you talking about, single pulse or clock? what is time rangeof pulse? Its a big difference if you need clock pulse in ms or in some seconds... regards |
12/5/2014 10:52 AM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
To add some new point to our friend Jens_app: To save extra timers, for pulse generation,I suggest using clock of CPU and just count the values.The whole scenario will be 16 seconds and reset when counter reach this point.Compare the count value and generate outputs (high=pulse) or (low=pause).
|
This contribution was helpful to1 thankful Users |
12/5/2014 11:37 AM | |
Joined: 1/5/2011 Last visit: 4/22/2024 Posts: 815 Rating: (121) |
I completely agree with huggy, there are many different approaches and by using the CPU clock you will save timers and memory. I've took the liberty to quickly write a program according to the hints our expert huggy gave us. This piece of code uses the CPU clock pulse and an integer that holds the amount of time a pulse is activated or deactivated. Pulse on -and off time can be adjusted. |
Keep it simple and on-topic. |
|
This contribution was helpful to1 thankful Users |
Follow us on