7/12/2013 7:56 AM | |
Joined: 10/3/2010 Last visit: 9/20/2024 Posts: 1562 Rating: (191) |
Not sure, just trying to give hints (attached)... or How can you use the OS project editor to copy user-specific pictures or modified template pictures into the currently opened OS project? AttachmentVBS-Language.pdf (244 Downloads) |
Last edited by: SteBo at: 7/12/2013 8:10 AMB r g d s , |
|
This contribution was helpful to1 thankful Users |
7/12/2013 12:04 PM | |
Joined: 10/3/2010 Last visit: 9/20/2024 Posts: 1562 Rating: (191) |
Hey Jake, there is a way that I think you could use. First add your texts in different languages into the Text Library (if you know WinCC Configuration Tool with Excel), it's easy to add those). Remember the ID's they will get in the Text Library Table. Afterwards, you can create Internal Tag(s) of the Text Reference-type and as Start Value, enter the corresponding ID from the Text Library. Now you can use this/these Internal Tags for dynamics on your screens. Check the link below for a little more detailed description with some sample screenshots. How can you configure process screens in multiple languages with WinCC text reference tags? Please also read this for reserving a rande of ID's in the Text Library to make sure that your own text are never shifted in the list. If you don't know the Configuration Tool, please check this manual |
Last edited by: SteBo at: 7/12/2013 12:19 PMLast edited by: SteBo at: 7/12/2013 12:13 PMLast edited by: SteBo at: 7/12/2013 12:07 PMadded extra link B r g d s , |
|
This contribution was helpful to2 thankful Users |
7/12/2013 12:36 PM | |
Posts: 165 Rating: (2) |
Thanks. I am not quite there to do this yet - but when I get to this, I'll follow your suggestions - and let you know how it went... Jake |
12/11/2014 12:24 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on