5/4/2013 12:24 AM | |
Posts: 123 Rating: (5) |
Hello everyone, I don't see a way to create a structure in WinCC (tia portal v12) like how it's possible with WinCC Flexible (2008). Is there a way?
|
5/6/2013 3:48 PM | |
Posts: 123 Rating: (5) |
Thank you Tweety |
This contribution was helpful to1 thankful Users |
6/5/2013 9:19 AM | |
Posts: 123 Rating: (5) |
When I use wincc structure to read data from the plc. Is the tag connection always absolut or it can made symbolic? |
6/5/2013 4:48 PM | |
Posts: 3037 Rating: (192)
|
Hello, Which PLC do you use? http://support.automation.siemens.com/WW/view/en/67582844 Tweety |
6/11/2013 10:36 AM | |
Posts: 3037 Rating: (192)
|
Hello, This is ok. You can only connect a UDT of the plc absolutely. Tweety |
This contribution was helpful to1 thankful Users |
5/12/2014 12:13 PM | |
Joined: 9/1/2005 Last visit: 5/10/2024 Posts: 4100 Rating: (193) |
follow up question published by kifihsis split to a seperate thread with the subject UDT in WinCC v12 Dint element with linear scaling property. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on