Industry Online Support
Technical Forum
12/3/2014 9:39 AM | |
Posts: 8946 Rating: (999) |
You may use thefunction StartProgram "myprogram" myprogram is your EXE - File. |
12/29/2014 3:39 PM | |
Posts: 18 Rating: (1) |
Thanks ! ! It worked. How can I find the project path in WinCC Flex script ? |
12/30/2014 9:04 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168)
|
Hello NitinG66, Perhaps this link might help: how do you open a WORD document via an operator panel? Best regards, Wizard |
12/30/2014 7:03 PM | |
Posts: 8946 Rating: (999) |
There is no tag. But you may use a fixed string if path will not be changed. Why do you need ist? |
12/31/2014 8:28 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168)
|
Hello NitinG66, Have you seen this link: how on a PC with WinCC flexible can you use a script to save and read out information in a text file? Best regards, Wizard |
12/31/2014 9:21 AM | |
Posts: 8946 Rating: (999) |
If you change project path, you must change also the start-up path on the new PC. So you will have some work to do anyway. a.) So you may create ainformation - File in root directory (C:\) and define the relevant pathes inside. You read this .TXT or .CSV file in a script by starting up the runtime and find out the pathes that you Need. If you change directories, you just have to change this Information - file once. b.) For me it do not seems very helpfull to put data files in project directory. Why you do not use a fixed directory "USERDATA_WCCFLEX" for your data? c.) You may use an environment variable in Windows. (but also has to change if path will change) d.) If you don't like this ideas, perhaps this link is helpfull ->Finding File<- Good luck! |
This contribution was helpful to1 thankful Users |
Follow us on