6/11/2011 7:29 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Just found this news: SIMATIC PCS 7 V7.1 SP3 http://support.automation.siemens.com/WW/view/de/50721458 (only in German for the moment).
SIMATIC PCS 7 V7.1 SP3 = SIMATIC PCS 7 V7.1 SP2 + small updates (not revolution) + Software components on the SIMATIC PCS 7 DVD V7.1 + SP3 (check in the link above).
|
Last edited by: UMENCHO at: 6/11/2011 7:31 PM |
|
This contribution was helpful to2 thankful Users |
6/11/2011 7:39 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Dear UMENCHO, Any idea when it is going to be released in English? |
VANDE MATARAM..... |
|
1/14/2015 6:52 AM | |
Joined: 2/6/2009 Last visit: 3/21/2024 Posts: 938 Rating: (118) |
Hi, Find the attcahment for complete compatability list of all versions of PCS7. AttachmentPCS-7_compatibility-list_en_2015-01-12.zip (346 Downloads) |
_______________________________________________________________ |
|
1/15/2015 5:43 PM | |
Posts: 2661 Rating: (279)
|
Hi AliNda, The latest version of PCS7 is V8.1 and it's primarily meant for Windows 7 and Windows Server 2008 platforms. See the following link: Delivery Release for SIMATIC PCS 7 Process Control System V8.1 Windows 7 based PCS7 versions began with V8.0. Additionally a new SP4 was released for PCS7 V7.1 to include Windows 7 support. Regards |
Follow us on