3/29/2012 5:34 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating: (71) |
Hi Gourav, this may be a timing problem. Check this FAQ: http://support.automation.siemens.com/WW/view/en/23061262 |
mfG / Best regards |
|
1/23/2015 8:08 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello Gourav, you have not told, which version of WinCC you are using. This error was known with WinCC V7.0 SP3 (without Update). It is solved with the actual Update, you should install the Update 6. http://support.automation.siemens.com/WW/view/de/81524617 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on