Industry Online Support
Technical Forum
2/2/2015 3:39 AM | |
Joined: 10/18/2014 Last visit: 11/28/2023 Posts: 95 Rating: (15) |
hello sir i am using wp231 for weiging in conveyor belt. object stay at load cell platform for less than 1 second almost upto 500 ms - 600 ms . i am not getting coreect value or accurate value there is every time differnece varying , sometime 1 gram , sometime 2 grams & some times it shows 4-5 grams variations. i have calibrated correctly but uable to get correct weight in running application. please help or suggest is it possible to measure running value with the help of wp231. there are continuosly back to back objects on platform, 1 egg for every 1 second. application is poultry farm egg conveyor.
------------ Splitted from WP231 - variation of 50g for the 25kg. |
Last edited by: Min_Moderator at: 2/2/2015 11:44 AMNew subject after splitting Ganesh-0220 |
|
Follow us on