2/1/2015 3:12 PM | |
Joined: 9/3/2008 Last visit: 9/19/2024 Posts: 928 Rating: (162) |
Hello, If I remember correcly, you need Simatic Net 8.2 or later installed. |
Michael |
|
2/2/2015 6:20 AM | |
Joined: 9/9/2007 Last visit: 8/12/2021 Posts: 27 Rating: (0) |
my simatic net version is 8.1+sp1 |
Last edited by: MDehshat at: 2/2/2015 6:22 AM |
|
2/2/2015 6:59 AM | |
Joined: 10/7/2005 Last visit: 9/21/2024 Posts: 3021 Rating: (1054) |
Hello MDehshat You can use the H-CPU's PN port for fault tolerant connections, but need to fullfill the following requirements: - CPU Firmware >= 6 (ok, PN H CPU's came out as V6.0) - Softnet >= V8.1.2 (you have 8.1.1) - Must have license for it and install S7-REDCONNECT from same Softnet CD -Must use ISO-on-TCP (can NOT use pure ISO with CPU's PN port) - CP1623 in PC (which you have) Have a look at chapter14.6 of the SIMATIC Fault-tolerant systems S7-400H for more on this. I hope this helps |
Last edited by: fritz at: 2/2/2015 1:40 PMupdated CPU firmware note Last edited by: fritz at: 2/2/2015 7:38 AMCheers |
|
Follow us on