Industry Online Support
Technical Forum
2/11/2015 8:20 AM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359)
|
Hello Ali Bostan,
Please find the help regarding Event ID 43D8 that occurred in your system as "Unilateral program execution error" in your H-system.About the module address "8252" , this is not a hardware address and this is the position of machine code in your CPU that error happened, and buffer guide you to the point but the block is protected .For further analysis, we need your project.Please contact me via "personal messages" if you have limitations to publish your project online. I hope this helps, Hamid Hosseini
Attachment43D8.pdf (231 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on