8/25/2014 9:31 AM | |
Posts: 14 Rating: (0) |
Hi all, We have IM 308-3UC1 in our system, how can we read out file .pb5 from memory card 5V FLASH 256? please! Thanks. |
8/25/2014 11:30 AM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046)
|
Hello dongta Firstly you need COM Profibus which is sadly not available as a free download (suggest you get in touch with your nearest Siemens rep who may be able to help you out). Thereafter you can either - upload the .pb5 file directly from the IM308C (via its Profibus port, you'll need a Profibus CP in your PC ora Siemens PG for this) OR - upload the .pb5 file from the EPROM itself (you need a Siemens PG or external EPROM reader for this and obviously take the EPROM out of the IM308C) Have a look at COM PROFIBUS and ET 200 Distributed I/O System with IM 308-C and S5-95U manuals for more details on the above. I hope this helps I hope this helps |
Cheers |
|
8/27/2014 4:21 AM | |
Posts: 14 Rating: (0) |
Thanks you very much. |
8/27/2014 9:44 AM | |
Posts: 14 Rating: (0) |
Hello Fritz, I already have PC installed COM Profibus. Please, what kind cable do I have to connect betwen PC and IM 308C? thanks for your answers. Cheers, dongta |
2/11/2015 4:22 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on