8/31/2011 2:52 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Yes, you can. Is it possible to attach here hardware configuration? Best regards, Hristo Mihalev |
8/31/2011 3:25 PM | |
Joined: 9/12/2008 Last visit: 10/21/2023 Posts: 73 Rating: (2) |
I export the hardware config. Ps. i checked the cfg file and i see:PDM_PARAM "0" I hope that means PDM is not used :)
Attachmentsimatic 400.zip (412 Downloads) |
6/17/2014 7:36 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
I also had this problem, but I don;t know how I solved it, not with reorganize. I try to find the solution. But what it means is that you inserted a PDM device into your hardware. For some reason, simatic manager still "remembers" you have a PDM device insertedand it asks for a license. I had this problem at PCS7 8.0 |
If I could help you, you can use the RATE button. Thank you. |
|
2/16/2015 4:56 PM | |
Posts: 1 Rating: (0) |
Hi, So is it correct to say that if you export your H/W config and the "PDM_PARAM = 0" there are no PDM used? Then it's safe to 'save as...' with reorganisation. |
Follow us on