1/29/2015 12:44 PM | |
Joined: 3/14/2008 Last visit: 3/29/2024 Posts: 2059 Rating: (924) |
Is the message class you have chosen supported in the russian PCS7 package?. If it is not supported, no messages will be created...Maybe you can change the message class and see if it works when you do a compile OS etc.. |
Last edited by: Oreca at: 1/29/2015 12:49 PMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on