3/9/2015 7:13 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello, You have done all time parameterization in a correct way but it is not clear when the output value of timer is written to TV?This is source of trouble and it is determined by the conditions (set of ANDs and ORs).If the current time value of Timer is S5T#0ms, the timer never start again even all triggering conditions are met. So what was your first idea,Did you want to make a time with pausing capability?I suggest reading this old topic for an On Delay timer with pause signal. Timer which does not reset itself I hope this helps, Hamid Hosseini |
Last edited by: hdhosseini at: 3/9/2015 7:14:51 PM |
|
Follow us on