3/9/2015 7:31 AM | |
Joined: 2/21/2014 Last visit: 3/14/2024 Posts: 652 Rating: (341) |
Hi, First you need to get the picture name assigned to PictureWindow1. Then you can easily assign the Properties to the Objects in that Picture. e.g. on click event of IO fields you can try this: char *pszPicture = NULL; //I am not sure what you want with the Bar object, but if you want to change the value on IO click, try this //50 is just an example. assign the value you want. "Value" is the property which should be changed in Bar. change it to the Property which you want to update. If you want to assign TAG to IO, e.g. Tag1 on IO1 click or Tag2 on IO2 Click, Then use SetLink function. Thanks, HarrY
|
You can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
3/9/2015 10:20 AM | |
Posts: 56 Rating: (0) |
Thank you HarrY ji, I want assign tag to bar1 for maximun value. SetLink(pszPicture ,"Bar1","Maximum Value",&linkinfo);// this is not working |
3/10/2015 3:32 AM | |
Posts: 56 Rating: (0) |
Thank you HarrY ji |
Follow us on