3/10/2015 4:25 PM | |
Posts: 15 Rating: (0) |
Dears, I need to use TIA portal V13 to create a PLC program for a “S7-300” PLC, the PLC will be communicating with a third party flow computer(Modbus TCP server) using Modbus/TCP. I’m using Siemens S7-OPENMODBUS/TCP V5 to establish Modbus communication between the PLC and the flow computer and I’m following the instructions in the manual of the openmodbus cd which are unfortunately for step7 and not TIA portal. My problem is that I can’t find any way to add the required “OTHER STATION“ to my hardware configuration (as described in the attachment pages 15 & 18) I even created the project in step7 and tried to use the migrate tool in the TIA portal to convert the project from step7 project into TIA project, but it failed to recognize the "other station" object. Also I can’t find any document for describing how to use OPENMODBUS/TCP with TIA portal I hope that anyone can help me with my problem, and thank you very much for your help and support.
Best regards, mMoussa AttachmentSIMATIC ModbusTCP for NCM_CP English.pdf (308 Downloads) |
3/10/2015 5:34 PM | |
Posts: 3093 Rating: (322)
|
Hello mMoussa, Regards, |
3/10/2015 11:39 PM | |
Posts: 15 Rating: (0) |
Dear Kaulquappe, Thank you for your reply, I really appreciate your help. Best regards, mMoussa |
Follow us on