3/11/2015 2:27 PM | |
Posts: 1 Rating: (0) |
Using the software SIZER to select the hardware and firmware components necessary to implement a drive task.
The drive system has five axes. The properties of this drive system are multi-axis converter, active line module.
One of the axes is spindle, the basic type of spindle motor is 1PH7288, the power of spindle motor is 260KW.
The other four of the axes are feed shafts. The basic type of each feed shaft is 1FT6108, the power of each feed shaft is 16.8 KW.
But when I use SINUMERIK 840D sl to configure as the controller for the above drive system, SIZER signals an error, which is “all assigned line and motor module are not approved for SINUMERIK”.
I want to know what are the main reasons for this error. Is it because the power of spindle motor is overload for SINUMERIK?
Can anyone advise any solution. It would change almost everything. Really going crazy about it now. |
Last edited by: monicagj at: 3/11/2015 2:35:42 PMLast edited by: monicagj at: 3/11/2015 2:42:01 PMLast edited by: monicagj at: 3/11/2015 2:56:13 PM |
|
Follow us on