3/12/2015 6:30 AM | |
Joined: 4/22/2014 Last visit: 4/27/2024 Posts: 20 Rating: (0) |
Dear Friends, I have upgraded my project from PCS78 V7.1 to V8.0 SP1 Upd1. On Server machine when i open Group faceplate i get "No Cemat PLC Found" popup message. I have 6 PLC's and I checked the System folder and all charts are version 8 and numbered as SYSPLC01,02....06. The wincc compile has no errors, i can see the Sytem tags for respective PLC also in wincc. The Cemat version i have used is Cemat V7.1 SP1 with HF120127 which is for Windows7 compatibility. My server is running on Windows Server2008 R2. I am not able to figure out what could be the issue. Please help me. Best Regards, Ram Kishore
------------ |
Last edited by: Min_Moderator at: 3/12/2015 12:26:13 PMNew subject after splitting |
|
3/12/2015 12:56 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Last edited by: Min_Moderator at: 3/12/2015 1:31:29 PM |
|
Follow us on