11/2/2012 4:05 PM | |
Joined: 10/31/2011 Last visit: 1/30/2024 Posts: 400 Rating: (5) |
Dear nmnogueira, I have proceed as you say now no address error but process value is zero
|
11/2/2012 7:00 PM | |
Joined: 10/31/2011 Last visit: 1/30/2024 Posts: 400 Rating: (5) |
Please see required registers of my device |
11/6/2012 10:06 AM | |
Joined: 3/15/2010 Last visit: 4/2/2024 Posts: 137 Rating: (9) |
According to the table you sent, the address 400001 should be correct. Please check if you have any voltage to be read |
11/7/2012 3:08 PM | |
Joined: 3/15/2010 Last visit: 4/2/2024 Posts: 137 Rating: (9) |
Just to confirm, are you using address 400001 (with 4 zeros)? |
11/10/2012 1:57 PM | |
Joined: 10/31/2011 Last visit: 1/30/2024 Posts: 400 Rating: (5) |
Dear Sir, I am using smae address 400002 and 400001 and give you connection status.
|
11/16/2012 4:43 PM | |
Joined: 10/31/2011 Last visit: 1/30/2024 Posts: 400 Rating: (5) |
Is there any further remedy..... |
3/16/2015 11:14 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
|
Follow us on