3/23/2015 10:06 AM | |
Posts: 19 Rating: (0) |
Hello Elonen, First I would like to thank you very much for your answer. Now I am trying myself to convert STL to LAD Logic. I am having SIMATIC MANAGER V5.5 and program backup which has one FB & 2 FC's. Most of the STL networks are converted to LAD using direct conversion option in SIMATIC MANAGER except two of them in FB. Please help me in converting these two networks to LAD. Here I am copying the STL logic. #Network 1: (Set Initial values Logic) L #ADR_IN L #ADR_OUT SET O( U #Input.ACT.SW.ALARM U #EXT_CTRL L 0 L #PPO_TYPE L #ADAPTER_TYPE L #DRIVE_TYPE SET U #DPV_MODE #Network 2: U #DPV_MODE
Thanks & Regards, Saidulu
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 3/24/2015 10:53:32 AMNew subject after splitting |
|
3/24/2015 6:39 AM | |
Posts: 19 Rating: (0) |
Hello, Can someone help me in converting above logic to LAD? This is very much important for me. Please help. Thanks in Advance.
Saidulu |
3/24/2015 10:55 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on