4/9/2015 9:38 AM | |
Posts: 7 Rating: (0) |
Hi, I have Control panel KTP600 Basic color DP. I have Wincc flexible Version 2008 SP1 software. and I have interface cable MPI/DP --------------------------------------------------------------------------------------------------- MPI/Profibus Settings in Control Panel: Station Parameters: Address: 1 Time-out: 1s Network Parameters: Transmission Rate:1875 KBaud Highest Station:31 Profile:MPI -------------------------------------------------------------------------------------------------- Communication settings in Wincc flexible: Device type: KTP600 Basic color DP. Mode: MPI/DP. Station address: 1 ----------------------------------------------------------------------------------------------------- I put the communication settings in Wincc flexible matching with MPI/Profibus Settings in Control Panel and I try to get project backup but not success. and I got this message (A connection could not be established. Please check your setting,ports,cable ect...). I already checked the connection and replased the cable but still the problem. And I follow these procedures: Procedure - Backup Proceed as follows: 1. Select the menu command "Project ▶ Transfer ▶ Communication Settings" in WinCC flexible on the configuration computer. The "Communication Settings" dialog opens. 2. Select the HMI device type. 3. Select the type of connection between the HMI device and the configuration computer, then set the communication parameters. 4. Close the dialog with "OK". 5. In WinCC flexible, select the menu command "Project ▶ Transfer ▶ Backup". The "Backup Settings" dialog opens. 6. Select the data to be backed up. 7. Select a destination folder and a file name for the *.psb backup file. 8. Set "Transfer" mode on the HMI device. If automatic transfer mode is enabled on the HMI device, the device automatically sets "Transfer" mode when a backup is initiated. 9. Start the backup operation in WinCC flexible with "OK" on the configuration computer. Follow the instructions in WinCC flexible. A status view opens to indicate the progress of the operation. ---------------------------------------------------------------------------------------------------- Can you help me pleaseeeeeeeeeeeeeeeeeeeeeeeeeee.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/9/2015 4:08:03 PMNew subject after splitting Last edited by: sale2h2002 at: 4/9/2015 5:03:16 PMLast edited by: sale2h2002 at: 4/9/2015 5:05:30 PMLast edited by: sale2h2002 at: 4/10/2015 9:17:55 AM |
|
4/10/2015 3:34 PM | |
Posts: 7 Rating: (0) |
Hello Murof My PG/PC interface Settings in my windows control Panel is: PC Adapter(Auto) could you see attachment |
4/10/2015 5:37 PM | |
Posts: 7 Rating: (0) |
Murof could you see another attachmen. |
4/10/2015 5:40 PM | |
Posts: 7 Rating: (0) |
another one |
4/10/2015 5:41 PM | |
Posts: 7 Rating: (0) |
|
6/12/2020 3:11 PM | |
Posts: 1 Rating: (0) |
Did you solve this? I have same issue. Please advice. |
Follow us on