4/12/2015 6:21 AM | |
Posts: 1 Rating: (0) |
Hello, I currently have a 414-H system with 2 6ES7414-4HM14-0AB0 and I have just updated them to firmware version 4.5.6.
The firmware update worked fine. I am trying to update a spare processor the site has that is not installed I am just trying to connect through my laptop directly to the processor to update the firmware so it is the same as the 2 that are being used. I cannot download a simple hardware config to the processor.
I can ping the processor what it is not available to do a hardware config to.
I have attached the simple project.
Any help would be appreciated.
Thanks,
Palmer Gobert Spencer Engineering AttachmentHW_Config.zip (410 Downloads) |
Follow us on