4/10/2015 11:32 AM | |
Joined: 2/10/2015 Last visit: 4/10/2024 Posts: 285 Rating: (1) |
hello everyone I try to transfer my program in my display TP177B DP-6 MSTN PC with a USB adapter cable (6ES7 972-0CB20-0XA0) and I edit my program with flexible wincc 2008 (v1.4.0.0_1.16.0.16) and I chose in wincc as MPI / DP communication mode and in my display I also chose MPI and 187.5kbits / s as the transmission speed, highest address as 31 and 10s as a waiting delay but when I click on transferring in wincc I see that the transfer does take place but I receive an error message (not possible to establish the connection. check your cable parameters, interfaces etc) .Please I need urgent help, thank you and good day to all. ----------------------------------------------------------------------------------------------------
Split form How to program FC9 and SFC1 in simatic Manager. |
Last edited by: Min_Moderator at: 4/10/2015 1:49:32 PMNew subject after splitting |
|
Follow us on