4/13/2015 5:43 PM | |
Posts: 4 Rating: (0) |
Hi all, I have a problem when I connect two wincc Server with S7 412-5H (Redunacy CPU). Please see attached file. I had config to connect wincc sever 1 with s7 400 successfull : + Create PC Station, insert s7_connection.. in step 7 + Import station on wincc server 1 PC ( have Redconect ) when I config to connect wincc server 2 PC same wincc server 1 PC, the wincc sever 2 can not read data from s7 400. I don't know the reason of this error. Please help me. Thanks. AttachmentErr.pdf (117 Downloads) |
4/14/2015 8:42 PM | |
Joined: 9/3/2008 Last visit: 4/24/2024 Posts: 920 Rating: (156) |
Hi, Did you create the S7 connection as "S7 fault tolerant" ?
|
Michael |
|
Follow us on