4/15/2015 12:05 PM | |
Joined: 3/16/2012 Last visit: 6/18/2024 Posts: 26 Rating: (0) |
Hii... i am using MODBUS_PN block for cpu 315 2 pndp, i can read the area of Yokogawa recorder DX1006, And i am able to write the only addresses from 1to 24, but for computation channel i need to write some more area , if i increse data lenght more than 24 then its Gives A095 error..
---------------------------------------------------------------------------------------------------- AttachmentAddress.zip (312 Downloads) |
Last edited by: Min_Moderator at: 4/15/2015 4:30:55 PMNew subject after splitting |
|
4/15/2015 12:12 PM | |
Joined: 3/16/2012 Last visit: 6/18/2024 Posts: 26 Rating: (0) |
Hi...i am using modbusTCP, for Cpu 315 2pn dp... here i used siemens standard block MODNUS_PN & other blocks , found connection established with master (yokogawa recorder DX1006)... but when i try to write data it gives A095 status which meainf is given below. Check the error message of the I think i am puting resister start & end address wrong or may there is some setting missing at master site... Please suggest , i have attached snaps from manual AttachmentAddress.zip (343 Downloads) |
Last edited by: Mayyu at: 4/15/2015 1:20:20 PM |
|
Follow us on