5/5/2015 5:03 AM | |
Posts: 2 Rating: (0) |
Hi, Good day. I having a problem with PCS7 module 6ES7 332-8TF00-0AB0 (Hart module), as I compile my project the Module Driver Log give the error: "E: AO8x16Bit HART (6ES7 332-8TF00-0AB0) is not supported" As I refer to the PCS7.0 SP1 release modules it state that this module is supported. For your refference I'm using PCS 7 V7.0 + SP1. While for the CFC chart for the Hart module AO, I'm using the same driver "CH_AO". for the Hardware Configuration I already add the "Hart Field Device" (in case this could be the problem) but still give me the same error. I really hope somebody can help me with this issues. Thank you in advance. AttachmentSIMATIC H LG_Module driver 20150505.txt (80 Downloads) |
Follow us on